;

/ WIDE BANDGAP CONTINUES TO DISRUPT

By Philip Ling, Technical Content Manager, Avnet

When we experience major shifts in the technology landscape, we should expect disruption and turbulence. OEMs, suppliers and distributors are coming together to navigate rough waters.

The shift from conventional silicon toward wide bandgap (WBG) substrates for power applications, predominantly Silicon Carbide (SiC) and Gallium Nitride (GaN), isn’t without its challenges. The supply chain for WBG solutions is now maturing, which means we’re seeing consolidation, acquisition and even some attrition.

This turbulence, while a cause for concern, is predictable and surmountable. Confidence in WBG technology remains high, but the market conditions and geopolitical risks must be acknowledged as contributing factors.

New applications are exhibiting polarized conditions. Demand for electric vehicles (EVs) has plateaued in some regions, while the thirst for AI data centers seems unquenchable. Both are served by WBG devices. The technological benefits of WBG are clear, but challenges around its use can still be a barrier. Recently, we asked SiC market leader onsemi for its thoughts and recommendations.

With a fully vertically integrated supply chain, from crystal growth to final packaging, onsemi is addressing scalability, quality control and cost efficiencies in-house. While it sees yield and the transition from 150mm to 200mm wafers as ongoing challenges, demand volatility can cause inventory fluctuations. This is a key contributor to the turbulence we’re seeing, but it's part of the natural evolution of new technology.

Partnerships with companies including Vitesco and Magna, and long-term agreements are part of onsemi’s strategy to secure supply and fund capacity expansion. Its recent acquisition of Qorvo’s SiC JFET technology and the United Silicon Carbide subsidiary further strengthened its position.

infographic about SiC devices

ADVICE TO OEMS

  • Secure long-term supply agreements and diversify sourcing
  • Collaborate early with suppliers and plan for extended lead times
  • Prioritize supply chain resiliency over technical specifications

FACTORS DELAYING SIC ADOPTION

  • Moving to SiC requires redesign, particularly for gate drivers
  • Higher switching speeds are good, but can lead to EMI problems
  • Component cost is still high, but savings are made at the system level
  • Fear of supply assurance

Why is SiC better than Si?

The impact of increased demand

As demand increases, higher volumes will drive down per-unit pricing, which justifies the investments being made in larger wafer sizes and new fabs. onsemi currently operates fabs and packaging facilities in multiple regions, helping to avoid supply chain disruptions related to geopolitical tensions and export controls.

As capacity expands due to demand, suppliers will see higher returns on their investments. This will support the industry’s virtuous cycle of investment in capacity. As technology matures, production volumes and yields improve and lead to greater process stability. Also, onsemi contributes to JEDEC (Joint Electron Device Engineering Council), Automotive Electronics Council (AEC) and the European Center for Power Electronics’ Working Group "Automotive Qualification Guidelines" (AQG) to define SiC standards, which promote stability and interoperability between suppliers.

Turbulence will give way to stability

WBG is a transformative technology. It brings benefits to critical applications, including EVs, AI data centers and renewable energy. The strategic investments being made by suppliers such as onsemi demonstrate the industry’s commitment.

Pairing the right technology to key applications is crucial. For example, data center power and circuit protection are applications where SiC JFETs are differentiated by their low on-resistance and switching frequencies, surpassing GaN and even SiC MOSFETs.

Market conditions and the challenges of adopting new technology are contributing to the turbulence we’re seeing in the market. But demand continues to grow, paving the way to stability.

How does SiC lower opex?

SiC & GaN Suppliers:

Silicon Carbide (SiC) MOSFETs, JFETs & Modules, SiC Schottky Diodes, GaN FETs

MANUFACTURER
TECHNOLOGIES
Bourns
SiC Schottky Diodes
Diodes Incorporated
SiC MOSFETs & Modules, SiC Schottky Diodes
Hirose Electric
SiC Schottky Diodes
Infineon
SiC MOSFETs & Modules, SiC Schottky Diodes, GaN FETs
Luminus Devices
SiC MOSFETs & Modules, SiC Schottky Diodes
Microchip
SiC MOSFETs & Modules, SiC Schottky Diodes
Nexperia
SiC MOSFETs & Modules, SiC Schottky Diodes, GaN FETs
onsemi
SiC MOSFETs, JFETs & Modules, SiC Schottky Diodes
Renesas
GaN FETs
Rohm
SiC MOSFETs & Modules
Sensitron Semiconductor
SiC Schottky Diodes
STMicroelectronics
SiC MOSFETs & Modules, SiC Schottky Diodes, GaN FETs
Teledyne e2v
GaN FETs
Toshiba
SiC MOSFETs & Modules
WeEn Semiconductors
SiC MOSFETs & Modules

BREAKING NEWS: GaN goes vertical

New vertical gallium nitride (vGaN) power semiconductors from onsemi set a new benchmark for power density. The company is now sampling 700V and 1200V devices to early access customers. Read more about this proprietary GaN-on-GaN technology.

ABOUT THE AUTHOR

Philip Ling

Technical Content Manager, Avnet


Philip develops content covering the full range of technologies supported by Avnet.

Philip has more than 30 years of electronics industry experience, including working as a design engineer on mixed-signal embedded systems. He was also a technical journalist and editor covering the industry for several European technical magazines. He has worked for small, medium and large companies as well as startups, and is pleased to say he is constantly learning.

He holds a post-graduate diploma in advanced microelectronics.